1/27/2021 9:48 PM | |||||||||
Joined: 11/2/2020 Last visit: 6/14/2023 Posts: 56 Rating: (3) |
How do I know which "image" (aka FIRMWARE) I need? I have a TP1200 Comfort panel and I downloaded 109746530_ComfortV2Panels_V16.0_Upd2.zip (76,9 MB) from https://support.industry.siemens.com/cs/us/en/view/109746530 and unziped it to C:\Program Files\Siemens\Automation\Portal V16\Data\Hmi\Transfer and replaced all. But when I right click the HMI in my project go to Download - Software (all) I get an error. "Fit - Components with a different version are installed on the target device." and there is a check box to "fit" it apparently (what does "fit" even mean here?). I can expand the error and there is another line "An older incompatible firmware image exists on the target device. If you update the operating system update, recipe data, user data and some system settings could be deleted permanently" with a check box to "Upgrade". Screenshot attached. Checking the upgrade box also checks the fit box. I press load and it says I am missing the images.
------------------------------------------------------------------------------------------ |
||||||||
Last edited by: Jen_Moderator at: 01/28/2021 10:33:19New subject after splitting. Optimized link |
|||||||||
1/28/2021 2:40 PM | |
Joined: 8/3/2009 Last visit: 7/15/2024 Posts: 13293 Rating: (1686)
|
Hello the best way at the moment with TIA Portal V16 ist to install the DVD3 "Panel Images" and then only the Update packages with all the Images from the FAQ: https://support.industry.siemens.com/cs/de/en/view/109746530 So to get the current Versions and Images: -> Basic-> Install V16 Panel images from DVD -> Install Upd 3 for TIA Portal -> Install the Upd3 Image Package from above FAQ Then you are uptodate Bye Murof |
If this Information really helps, you could use the Rate function |
|
1/28/2021 2:42 PM | |
Joined: 11/2/2020 Last visit: 6/14/2023 Posts: 56 Rating: (3) |
Um...Installed Software -> Detailed Information shows TIA Portal Project Server version is v16.0. I found one that appears to work. Using the link: https://support.industry.siemens.com/cs/us/en/view/109746530 and I downloaded SIMATIC_WinCC_Panel_Images_V16_Upd3a.exe (337,8 MB) and it actually had a.fwf that I could use. There are just SO many links and even though I have a "Comfort" panel the file under the "2.4 Comfort Panels, Comfort Panels Outdoor and Comfort Panels INOX" the zip file contained a .ruf file...which is apparently not what TIA wanted. There should be some way I can search my model and software version to find firmware instead of guessing which link I need to use.
|
Last edited by: Jen_Moderator at: 01/29/2021 08:09:33Optimized link. |
|
Follow us on