10/19/2022 4:20 AM | |
Joined: 4/7/2015 Last visit: 7/26/2024 Posts: 5 Rating:
|
I need to configure old MP277 panels with a new project from scratch, to communicate with new S71200 PLC’s (programmed in TIA V17). I understand the old HMI will not be able to be integrated into the existing TIAV17 project of the PLC’s, therefore the HMI will need to be its own project. My question is, what is best, should I configure siemens MP277 in winCC flex 2008 SP5, or the newest version of TIA that was compatible with the old MP277? (I.e. TIA V14) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/19/2022 05:45:26New subject after splitting |
|
10/19/2022 4:54 AM | |
Joined: 12/18/2014 Last visit: 8/16/2024 Posts: 33572 Rating:
|
Please don't post twice for the same problem. You also have make a own topic: MP277 panels new project - Should I use WinnCC Flex 2008 SP5, or TIA V14 (the latest TIA version to support MP277 panels)
|
This contribution was helpful to
1 thankful Users |
10/19/2022 5:46 AM | |
Joined: 6/19/2017 Last visit: 8/5/2024 Posts: 8175 Rating:
|
Closed cause question posted twice. The second thread with the subject MP277 panels new project - Should I use WinnCC Flex 2008 SP5, or TIA V14 (the latest TIA version to support MP277 panels) is published within the conference SIMATIC Panel. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on