11/20/2008 11:30 AM | |
Joined: 5/8/2006 Last visit: 4/29/2024 Posts: 1085 Rating:
|
Hi, Why do you not usea Ethernet CPon the rack withthe CPU 315-2DP? Another way is to usea OPC connection between the MP277 and WinCC PC. The MP277 can work as OPC XML Server and WinCC can work as OPC DA Client. Additionally you need an OPC XML-Gateway on the WinCC PC which converts the data of the OPC DA Client to the OPC XML Server. Maybe this FAQ will help you - see Fig. 02: http://support.automation.siemens.com/WW/view/en/25677751 Bye |
Follow us on