9/6/2024 11:39 AM | |
Joined: 4/1/2013 Last visit: 9/27/2024 Posts: 61 Rating: (3) |
I have the same issue, but I successfully communicated S7-1515T-2PN with 1756-L71 for both send and receive with DB_Data size of 100 bytes and with data length of 16 bytes. The setup I have is 1756-L71 is the server and the S7-1515T-2PN is the client. The problem I face is the moment I sent a 4byte size data (DINT, REAL) from 1756-L71 PLC to S7-1515T-2PN it does not receive fully the data or the data received is wrong and the following byte address from the byte address I configure to receive are not working at all. I configure from S7-1500 side to receive a 4byte size data from 1756-L71 and the by address I used is byte0, it should write the data from byte 0 until byte 3 since it is 4bytes of data but that's not happening. Furthermore byte address 4 onwards are not working once I start transferring 4 bytes size data to byte address 0 from 1756-L71 to S7-1515T.
------------------------------------------------------------------------------------------ AttachmentT_COMM status.zip (122 Downloads) |
Last edited by: Moderator_Lan at: 09/06/2024 11:56:48New subject after splitting "Never take advantage of others, but don't let others take advantage of you" |
|
9/6/2024 12:08 PM | |
Joined: 3/30/2020 Last visit: 9/26/2024 Posts: 4796 Rating: (984) |
Recently I tried to use T_COMM and did not succeed. I am currently using CIP Client and is happy with it. It is a one sided configuration and there is feedback (good/bad) if the data is usable. One drawback is that it may take up to 3 minutes or so to establish communications initially. There is also the need to detect if communication is failing. Communication needs to be broken down and built-up again when communication failed (partner disconnected). Attachmentcode-sample.txt (103 Downloads) |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on