7/25/2020 2:19 PM | |
Joined: 10/21/2015 Last visit: 5/21/2024 Posts: 2 Rating: (0) |
Hello to all. I already broke my brain while searching for a solution to my problem. Maybe you will have thoughts on how to solve this. Several years ago I could transfer projects WinCC OP270 for production without leaving my office, but at some point I did not have this function/ My work laptop is in "Industrial Ethernet" and the operator panel WinCC OP270 find in on "Profibus AUBO" with address 4. When trying to load a project, the following message appears (see screenshot) What can I try to do to solve this problem? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/27/2020 11:17:35New subject after splitting |
|
9/4/2020 1:56 PM | |
Joined: 8/3/2009 Last visit: 5/27/2024 Posts: 12984 Rating: (1654)
|
Hello I think you want do load the Panels with S7 Routing (From Ethernet to DP) Here are some information: https://support.industry.siemens.com/cs/ww/en/view/32235096 I hope it helps bye Murof |
If this Information really helps, you could use the Rate function |
|
11/6/2020 11:05 AM | |
Joined: 3/27/2012 Last visit: 5/30/2024 Posts: 179 Rating: (4) |
Thats exactly what Siemens Engineer told you in above Reply |
2/15/2024 7:23 PM |
|
Joined: 11/19/2013 Last visit: 5/28/2024 Posts: 10 Rating: (1) |
No.. it wasnt |
Follow us on