4/14/2014 8:11 PM | |
Joined: 3/20/2013 Last visit: 8/5/2024 Posts: 3 Rating:
|
Hi its possible from Firmware version v4 see link https://www.automation.siemens.com/mcms/programmable-logic-controller/en/simatic-s7-controller/s7-1200/cpu/pages/default.aspx?HTTPS=REDIR Best regards Piet van Moort |
5/14/2014 3:32 AM | |
Joined: 4/11/2011 Last visit: 7/16/2024 Posts: 132 Rating:
|
There is nothing about 6 PTO-s. And in system manual update too.
|
I'm just a human. Mistakes are allowed. |
|
5/14/2014 5:44 AM | |
Joined: 11/21/2007 Last visit: 7/7/2024 Posts: 2325 Rating:
|
Hello Ravi Teja Pabolu You can use the Following : ET200S 2-Pulse O/P Module 6ES7138-4DD01-0AB0 - 3 Nos. for 6 Pulse Outputs SIMATIC DP, ELECTRONIC MODULE FOR ET 200S, 2 PULSE PULSED GENERATOR AND TIMER MODULE, 15 MM WIDE, 2 CHANNELS ( Upto 10 kHz ) For CPU you can use: CPU IM 151-7 SIMATIC DP, IM151-7 CPU FOR ET200S, 128 KB WORKING MEMORY INTEGR. PROFIBUS DP INTERFACE (9 PIN SUB-D, FEMALE) AS DP SLAVE, W/O BATTERY SIMATIC MMC REQUIRED or CPU IM151-8 SIMATIC DP, IM151-8 PN/DP CPU FOR ET200S, 192 KB WORKING MEMORY, INT. PROFINET INTERFACE (WITH THREE RJ45 PORTS) AS IO-CONTROLER, W/O BATTERY MMC REQUIRED to implement this system Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
5/14/2014 12:04 PM | |
Posts: 5225 Rating:
|
Hi there. That case was handled here: LINK The software allow you to only create 4 PTOs regardless of which outputs you use. "Navnag" has profided valuable information. I however have a naughty feeling that in costs it will be cheaper to use x2 S7-1200 PLCs. You can have x2 CPUs .. one can even be a CPU1211. The CPUs can be linked with Profinet.. if required. Maybe do some costings before coming to a final conclusion. Greetings. w |
This contribution was helpful to
1 thankful Users |
5/14/2014 1:49 PM | |
Joined: 11/21/2007 Last visit: 7/7/2024 Posts: 2325 Rating:
|
Hello William B For sure 2 Nos. S7-1200 would be costing less than the hardware proposed by me. However it would be a tad more complicated to program, commission and troubleshoot, especially when the six outputs are closely linked to each other requiring, a little more amount of programming. We must evaluate the total cost Hardware + Software + commissioning and decide accordingly. Cheers Navnag |
Last edited by: Navnag at: 5/14/2014 1:51 PMThere is no such thing as the last bug in a program |
|
Follow us on