4/18/2023 6:27 AM | |
Joined: 10/11/2006 Last visit: 6/25/2024 Posts: 5869 Rating:
|
Hello, speedsetpoint + additional torque limiting or move to fixed endstop has the same effect as torque control, and you can easily switch. 8.17.3 MC_TorqueLimiting V7 (S7-1500, S7-1500T) 8.17.3.1 MC_TorqueLimiting: Activate/deactivate force/torque limit / fixed stop detection V7 (S7-1500, S7-1500T) With the Motion Control instruction "MC_TorqueLimiting", you activate and assign parameters for force/torque limiting and fixed stop detection. Together with a position-controlled motion job, a "Travel to fixed stop" can be realized with the fixed stop detection. In the axis configuration, you can configure whether the force/torque limiting is to relate to the drive side or the load side. The functions of the Motion Control instruction "MC_TorqueLimiting" can be activated and deactivated before and during a motion job. https://support.industry.siemens.com/cs/ww/en/view/109812057 |
With best regards, |
|
Follow us on