8/31/2023 8:22 AM | |
Joined: 1/21/2013 Last visit: 7/10/2024 Posts: 2965 Rating:
|
Hi stu, Sancruz is right, a router (Layer 3 functionality) is needed to connect different subnets. However, the SCALANCE XC-200 family (as well as the XF-200G and XP-200) supports some Layer 3 functionality such as VLAN and NAT. In my opinion, it should be possible to configure the switch as a NAT router. Unfortunately, I cannot find an example of how to do this. Maybe examples for other devices like "How do you use a SCALANCE XM-400/ XR-500 as NAT router?" will help. However, this example is a bit older and it is important to know that the XM-400 or XR-500 devices support much more Layer 3 functionality. But it might be worth a try to use this documentation. Kind regards |
This contribution was helpful to
1 thankful Users |
8/31/2023 8:28 AM | |
Joined: 6/12/2019 Last visit: 10/30/2023 Posts: 11 Rating:
|
hi thanks i will investigate this option , thanks again stu
|
8/31/2023 9:26 AM | |
Joined: 12/16/2022 Last visit: 7/9/2024 Posts: 8 Rating:
|
SCALANCE XB-200/XC-200/XF-200BA/XP-200/XR-300WG Web Based Management V4.3.1 (siemens.com) |
This contribution was helpful to
1 thankful Users |
Follow us on