2/11/2011 9:54 PM | |
Posts: 30 Rating: (1) |
You have answered the question how much. The next question is how fast. 2 ms, 20ms, 200 ms, or 2 seconds? |
2/11/2011 11:28 PM | |
Joined: 3/31/2006 Last visit: 4/24/2024 Posts: 39 Rating: (1) |
It can be good 200ms! |
2/11/2011 11:29 PM | |
Joined: 10/7/2005 Last visit: 6/8/2024 Posts: 3008 Rating: (1051)
|
Hello uccilon you surely can do data exhange between these two S7 stationsand usage of GET/PUT in the PN/DP CPU via an unspecified connection to the 343-1 LEAN based CPU is whatI would suggest you implement. For more details on how to do this, allow me to direct you to THIS forum post, the only thing missing from it is the link to manual below which is a good reference document to have in general. CPU-CPU communication with SIMATIC controllers (compendium) I hope this helps |
Cheers |
|
2/12/2011 7:37 AM | |
Joined: 3/31/2006 Last visit: 4/24/2024 Posts: 39 Rating: (1) |
Thanks a lot, I will try to do something on Monday. |
Follow us on