11/16/2014 6:57 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307)
|
Hello nandgate CP 343-1 supports Server Functionality on S7 Connections . That means that you can usenit as a Server and use GET / PUT in 315-2 PN/DP to read / write data from CPU 313C Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
11/17/2014 7:12 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307)
|
Hi nandgate Yes ! CP 343-1 Lean supports lesser functions than CP343-1 ( e.g. It does not support Profinet Controller Functionality ). But, not to worry, it supports S7 communication with Server Functionality, which is sufficient for your requirement of data exchange with CPU 315-2 PN/DP. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
11/17/2014 1:58 PM | |
Posts: 319 Rating: (9) |
Hi Naveen, Thanks for the reply. I need a small clarification, what does S7 Server and S7 Client mean? Thanks and regards, nandgate.
|
11/18/2014 4:04 AM | |
Joined: 10/7/2005 Last visit: 6/6/2024 Posts: 3008 Rating: (1051)
|
Hello nandgate have a look at the thread how to communicate between CPU315-2DP with CP 343-1 lean and IM151-8 PN/DP CPU, it should contain all theinfo you are after. |
Cheers |
|
This contribution was helpful to2 thankful Users |
Follow us on