9/5/2014 5:58 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating:
|
Hello saeedplc Set PG/PC Interface allows you toconfigure the communication between the PG/PC and the PLC / Drives / HMIs / other Siemens devices. Using this we select the actual communication hardware and the protocol using which various Siemens Softwares will communicate with PLCs and other devices. Here we define the application that is going to access this Interface. e.g. STEP7 / Wicrowin / WinCC etc. Here again the available options are listed. |
There is no such thing as the last bug in a program |
|
10/18/2017 9:05 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by Mak4Siemens is split to a separate thread with the subject Not able to get desired PLCs when trying to browse trough 'Edit Ethernet node' option from Simatic. Best regards |
Follow us on