8/31/2018 1:18 PM | |
Posts: 18 Rating: (0) |
Hi, I use a CP 1542SP-1 IRC V2.0 with Protocol IEC 60870-5-104. Is it possible to set status IDs manually from the PLC program? If i send a "floating point"<36> and want to set flag SB when i have a manual value on a broken sensor or IV when i have a communication problem with a sensor. How do i do it?
Reference to page 94 of the oprating manual C79000-G8976-C426-04 https://cache.industry.siemens.com/dl/files/690/109741690/att_949320/v1/BA_CP-ET200SP_76.pdf AttachmentBA_CP-ET200SP_76.pdf (47 Downloads) |
Last edited by: Jen_Moderator at: 8/31/2018 1:27:09 PMAdded file from link as an attachment. |
|
Follow us on