12/19/2019 11:46 AM | |
Joined: 11/14/2018 Last visit: 10/31/2023 Posts: 502 Rating: (69) |
Hello Lionel90, just to clarify your intention, do you want to know, if you can use a HMI Panel to access a webserver which is running somewhere else in the network? So, that the HMI Panel is acting only as a client to the webserver. OR if it is possible to use the HMI Panel itself as a webserver (this is also possible) If you mean the first, which I guess you do, than I cannot say for sure. if you men the second, here is an application example for that: Greetings, Nzett11 |
If I could help you, be so kind and rate my contribution. :) |
|
Follow us on