4/23/2011 1:11 PM | |
Posts: 20 Rating:
|
Hii. I am facing a problem regarding this issue, I am using VMware Workstation V7.0. I want to connect to a PLC network (1 CPU and 1 ethernet CP) through VMware using Bridge connection. The problem is that when I ping to that ip address of the CP inside the VMware I get a reply but I get nothing in the accessible nodes either through Industrial ethernet or TCP/IP as S7ONLINE. i am using bridge connectionwith my network card at VMnet0,host connection with VMnet1 and NAT with VMnet8. and the ip range inside VMware I use 192.168.XX.XX and for PLC network I use the ip range 10.0.91.XX. I am using windows XP sp3 in the host machine and the operating system which i use inside the vmware is windows xp sp2 so, what i have to do to access s7 plc through vmware. Thanks in advance. Splitted from S7ONLINE over ethernet with VMWare?. |
Last edited by: O_Moderator at: 4/26/2011 11:24 AMnew subject after splitting |
|
11/30/2011 12:17 AM | |
Posts: 5822 Rating:
|
Dear Kevlar, I admit, I use STEP 7 V 5.5 SP 1 on a Win XP SP3VMWare (Player version). It works really great. How did you configure your network setting in the VM Ware? Do you use Bridge mode? I would also strongly recommend to you to install the SP 1 of STEP 7, you will find it at: Service Pack 1 for STEP 7 V5.5 and STEP 7 Professional 2010 maybe this will fix some issues. Best regards J_Bell |
1/17/2012 3:22 PM | |
Joined: 7/18/2011 Last visit: 10/9/2023 Posts: 521 Rating:
|
Hi raghuk, Did you checked local connection of PC adapter is set to USB ? Kind regards BV |
1/17/2012 3:39 PM | |
Posts: 5822 Rating:
|
Hello, BeVee is right. I also wonder where did you connect the USB Adaptor to on the S7 side? Can you see any LED lit on the USB Adaptor? Best regards J_Bell |
1/17/2012 4:31 PM | |
Posts: 65 Rating:
|
Hi, Where to check Local connection of PC adaptor. In Set PG/PC interface all the Drivers are there. And all LED's are glowing and not blinking. Regards, Raghu
|
Follow us on