2/19/2020 2:38 PM | |
Joined: 8/3/2009 Last visit: 5/3/2024 Posts: 12882 Rating: (1643) |
Hello do you use TIA Portal V16 and the latest Firmware for the S71500? If no then this nis not possible, because you need a IP Router. The S71500 in the not newest FW can only handly S7 Communication and HMI Transfer, but no common IP routing like VNC. Here you can see the news: https://support.industry.siemens.com/cs/de/en/view/109771626 Check here the slides -> Page 33 and following Bye Murof |
If this Information really helps, you could use the Rate function |
|
2/1/2022 2:18 PM | |
Joined: 9/29/2020 Last visit: 5/24/2022 Posts: 1 Rating: (0) |
The "latest" is not a version. Can you specify a version please. |
2/3/2022 11:52 AM | |
Joined: 8/3/2009 Last visit: 5/3/2024 Posts: 12882 Rating: (1643) |
Hello NotMyCircus first Offtopic: ------ I think a 2 stars rating is not very fair, because the answer is correct! ------ -> The IP Routing works in S71500 since Firmware V2.8 and the corresponding TIA Version V16 (or of course newer Versions). Here are some details: https://support.industry.siemens.com/cs/de/en/view/109773506/130169166859 Bye Murof |
Last edited by: Murof at: 02/03/2022 11:53:45If this Information really helps, you could use the Rate function |
|
Follow us on