5/10/2023 8:38 PM | |
Joined: 3/13/2012 Last visit: 8/30/2024 Posts: 5 Rating: (0) |
Same here. How do I add PROFIsafe to the PNPN 6es7158-3ad10-0xa0 coupler in TIAP V15.1? There is no ProfiSafe Type in "transfer mapping" ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/11/2023 09:52:46New subject after splitting |
|
5/11/2023 4:52 AM | |
Joined: 3/11/2019 Last visit: 10/11/2024 Posts: 1592 Rating: (289)
|
Hi, as already written in the other post and in my post above yours in this thread....
Or try to configure via GSDML, after installation the coupler is also available in folder "other field devices", but as mentioned above, it is not necessary. PROFINET GSD files : Gatewayregards sancruz
|
Last edited by: sancruz at: 05/11/2023 04:57:06Feedback appreciated, please rate |
|
This contribution was helpful to1 thankful Users |
5/11/2023 9:53 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Add PROFIsafe to the PNPN 6es7158-3ad10-0xa0 coupler in TIA V15.1 is published within the conference Communication / Networks. Jen_Moderator |
Follow us on