11/2/2005 12:23 PM | |
Joined: 8/25/2005 Last visit: 3/21/2024 Posts: 1161 Rating: (110) |
Hello, I only can give you a few informations. The IE/PB-Link you are using is made for the "CBA" communication. To realize the hardwareconfiguration you need the Tool STEP7 and iMap. With STEP7 you have to make a hardwareconfiguration with an CPU as DP-Master, generat a socalled "Component" and import this in iMap. If you want to make your Configuration using PROFINET IO you have to use the IE/PB-Link with the MLFB 6GK1411-5AB00. With STEP 7 V5.3 SP1 or better STEP7 V5.3 SP2 you can make your Hardwareconfiguration only with STEP7. Sorry, I don't know anything about MM440 [:(] Please check whether it is working as a DP-Slave, a DP-S7-Slave or a DPV1-Slave. Only the newest Version of the IE/PB-Link (ROFINET-IO) can be used as an DPV1-Master. Here are some links with further informations:
Hope this helps Best regards Sabine |
Follow us on