4/3/2024 10:32 AM | |
Joined: 2/9/2024 Last visit: 4/8/2024 Posts: 1 Rating: (0) |
Hi. Was there a solution to this? I have same problem. Can search for BACnet devices, I find it, but cant read the objects. The "server" is a Logic machine, and when i us BACnet Browser i can see all the objects. I've tried to connect to a Simens PCX, and then I find all the objekts without any problems. So im guessing the setup of the PN/BACnet Link is correct, and the problem is the Logic Machine. But dont understand what.... And having no luck importing EDE file, gets an error and tell me to check file. ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_9866679 at: 04/03/2024 13:22:26Last edited by: Jen_Moderator at: 04/04/2024 07:27:47New subject after splitting |
|
Follow us on