6/28/2018 9:05 AM | |
Joined: 8/10/2009 Last visit: 5/19/2024 Posts: 166 Rating: (2) |
Hi Anil Belkery , Were you able to solve your problem ? Thanks Manku ------------------------------------------------------------------------------------------ |
Last edited by: ssmanku1699 at: 6/28/2018 9:14:14 AMLast edited by: Jen_Moderator at: 7/2/2018 10:37:59 AMNew subject after splitting |
|
6/30/2018 9:55 AM | |
Joined: 8/10/2009 Last visit: 5/19/2024 Posts: 166 Rating: (2) |
Dear Mr Duris , Will there be a BUS FAULT : If there are two CP 343-1 Lean in one network and the Object name is same but different IP's : 1st CP : Name :cp-343-1-lean Mac Address : 00-1B-1B-39-39-A2 IP Address : 10.1.41.11 Subnet Mask : 255.240.0.0 2nd CP : Name :cp-343-1-lean Mac Address : 00-1B-1B-37-C9-60 IP Address : 10.1.26.11 Subnet Mask : 255.240.0.0 Both the IP's are pinging from the laptop being in the same network . [snip] Thanks Sarabjot Singh Manku [snip] AttachmentDiagnostic buffer of module CP 343-1 Lean.txt (36 Downloads) |
Last edited by: Jen_Moderator at: 7/2/2018 10:36:25 AMAdded diagnostic buffer as an attachment. Deleted phone number, because doesn't comply with forum terms. |
|
7/2/2018 10:39 AM | |
Joined: 6/19/2017 Last visit: 6/6/2024 Posts: 8145 Rating: (165) |
Closed cause question posted twice.
|
My Forum is the place to personalize your profile, |
|
Follow us on