10/19/2012 6:18 AM | |
Joined: 3/2/2009 Last visit: 5/28/2024 Posts: 94 Rating: (8)
|
Hello smitnh76, replace the faulty drive with a new drive of the same type and capacity to return to the secure RAID1 status after a fault. We highly recommend to use Siemens spare parts.You can choose to reboot the device. In this case, the RAID software automatically integrates the new hard disk - necessary if you have non-removable drives. For hot-swap drive you can use the "Rescan for Plug and Play Devices" command to synchronize the RAID system. Please have a look at the operating manual |
Follow us on