1/23/2020 11:24 AM | |
Joined: 7/5/2013 Last visit: 5/8/2024 Posts: 3083 Rating: (505) |
Hello Ankit, the following FAQ provides description and example to read from a file and write to a file. Try to create the code according your requirements and post it, if you need some help. With SIMATIC WinCC (TIA Portal) on a panel, how do you access process data in a file via a script? In the script they define a delimiter to separate the columns. Using that one, you can select your three columns from the file. Regards, Frink |
Pi is exactly three! |
|
Follow us on