9/12/2019 10:24 AM | |
Joined: 2/27/2015 Last visit: 10/17/2024 Posts: 1 Rating: (0) |
Hi¡¡¡, I tried to clone the SSD harddisk(Intel SSDC2BB080G4) of the PCU50.3 ------------------------------------------------------------------------------------------ |
Last edited by: U_62e75b93-ee3e-4999-aa65-8c3113ab0cfa at: 09/12/2019 10:25:34Last edited by: Jen_Moderator at: 09/12/2019 13:26:29New subject after splitting. Edited text for better reading. |
|
This contribution was helpful to1 thankful Users |
9/16/2019 8:10 AM | |
Joined: 10/17/2007 Last visit: 11/15/2024 Posts: 4074 Rating: (357)
|
Check which Ghost version you used V7.xx or V8.xx Or try other Clone sw Or bring the SSD and source HDD or SSD to computer shop pay them to do clone It is not belong to Siemens support frame
|
If you like my comments please |
|
8/5/2024 8:08 AM | |
Joined: 9/4/2017 Last visit: 11/13/2024 Posts: 7 Rating: (0) |
Hi I used ghost to clone a hard disk and used it on 840c and I have this error . Could you solve your problem? |
10/31/2024 12:56 PM | |
Joined: 5/17/2022 Last visit: 10/31/2024 Posts: 1 Rating: (0) |
For cloning, I always use a cheap clone dock from Amazon. Something like this:FIDECO Docking Station, USB 3.0 Hard Drive Docking Station for 2.5 and 3.5 inch SATA HDD or SSD, Support Offline Clone, TF & SD Card Reader, and 2x 18TB Hard Drives : Amazon.co.uk: Computers & Accessories It will make a verbatim copy of anything, without a PC. Just ensure the following: PUT THE CORRECT DRIVE IN THE CORRECT SLOT!! If you get the source and target drives in the wrong slots you will erase the source drive. Make sure you have a new target drive that is the same size or bigger or else you will get a fault. |
Follow us on