9/12/2022 3:45 PM | |
Joined: 9/5/2020 Last visit: 1/6/2024 Posts: 49 Rating: (0) |
Hi everyone, I have S71200 Siemens PLC and I want to communicate with Beckhoff bk9000 over TCP/IP. I used MB_CLIENT block and the "STATUS" was "0000" that mean it connected successfully. and when I change the data in DB block that I send the reserved data to it, they return to 0000 so their other thing that write to block which is the MB_CLIENT. The problem is the physical input did not refer to received data, and according the Beckhoff bk9000 manual; the first input data address 400001. what is the problem with this system? Is the address is incorrect? The following attachment represent to what I did.
AttachmentDoc1.pdf (64 Downloads) |
Follow us on