12/22/2020 10:42 AM | |
Posts: 2 Rating: (0) |
Hello J_Bell, I am facing issue with communicating S7-319 3PN/DP with S7 1516-3PN/DP. The S7 319 PLC has the add-on CP card mounted on it. CP 343-1 Lean is used with S7 319-3PN/DP PLC. PLC Details: 1. MES PLC - S7 1516 3PN/DP 2. Line PLC - S7 319 3PN/DP with CP 343-1 Lean we have to establish the communication between these two PLC through the CP card. CP 343-1 lean is directly connected to the X2 interface of the MES PLC through Ethernet. At Line PLC, the FC5 (AG_SEND) & FC6 (AG_RECV) is Used for connection & data transfer. what communication block/function we need to develop at the MES PLC side? We have used the TCON/TDISCON T_SEND/T_RCV blocks. Even though connection could not be established. Please suggest any other approach or what changes do we need to do at the Line PLC side. Much appreciate the response....:) Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/22/2020 13:42:17New subject after splitting |
|
Follow us on