4/4/2011 9:56 AM | |
Posts: 316 Rating:
|
Hi Frederik, If you use the "T_CONN" block you need no connection in NetPro. What for HW do you use? What will happen, when you change the input value of T_RECV Len to 100? |
4/4/2011 12:23 PM | |
Posts: 23 Rating:
|
That's the problem. My T_CONN gives no done, busy or error signal. The status of T_CONNis 16#0009 but i don't now what it means. In network 3 (Set_TCP_ENDPOINTx) i set this parameters: |
4/4/2011 1:02 PM | |
Posts: 316 Rating:
|
Just at this moment I see, you use a CP for communication? |
4/4/2011 1:28 PM | |
Posts: 23 Rating:
|
If i use this program (Link below) will it work then? |
4/4/2011 3:16 PM | |
Posts: 316 Rating:
|
You have to create a connection in NetPro.
The you can use the AG_x blocks. |
4/4/2011 3:54 PM | |
Posts: 23 Rating:
|
I' ve got a problem in the FC5(AG Send) block. The error is: 16#80B0 what means that the module the data record not recognize, do you now what it means? I've made in netpro a TCP configuration with a unspecified component. In the attachment you find the pictures of theconfiguration. The port in Deplhi is 3000, the IP is 192.168.200.130. The IP of the CPU is 192.168.200.124. The DB that i wan't to send and receive is 296 bytes, is that a problem?I hope you can help me. I will upload the other pictures. |
4/4/2011 3:55 PM | |
Posts: 23 Rating:
|
Second picture |
4/4/2011 3:56 PM | |
Posts: 23 Rating:
|
Third picture |
4/4/2011 3:57 PM | |
Posts: 23 Rating:
|
Fourth picture |
Follow us on