9/7/2022 12:44 PM | |
Joined: 2/11/2021 Last visit: 6/8/2023 Posts: 1 Rating: (0) |
Hello everybody, First, here's the context : For one of our futur trade fair, we were offered to be part of a connected virtual factory project by using the UMATI connected system (https://umati.org/). It allows us to exchange our datas with the system by using OPC UA. To do so, the UMATI system needs to connect to our machines by using a VPN connection and this is what I'm working on for now. To connect our machines, we are usually using a SCALANCE S615 for all of our connected application, so I'm using the same device to establish the connection as an OpenVPN Client to access to the Umati's OpenVPN Server. I configured the OpenVPN client of the SCALANCE as it is described on the .ovpn file generated by the server (see the .txt attachment ... I took off the certificates values for security reasons of course ... ). Also, I generated the .key (for TLS key) and the .crt (CA Certificate) with the keys available on the .ovpn file to fill them on the SCALANCE. Moreover, I followed some tutorials available on the Application Examples of the product but they are mainly dedicated to the SINEMA RC solution and now I'm stuck ... the device achieved to reach the server but it's then instantly disconnected for some reasons : [snip] Here is my OpenVPN client configuration on the SCALANCE S615 : [snip] I checked the firewall of the SCALANCE and the main firewall of our factory, everything seems to be okay. I noticed that on the authentification method, I can't choose something else than "Username/Password" while I don't get it on the configuration file send by the OpenVPN Server ??? Moreover, I can't choose any other authentification method like "Certificates" for example, I've got a error message on this case and I can't set the connection to "Start" " Anyone has any advice about this issue ? Thanks in advance AttachmentFiles.zip (53 Downloads) |
Last edited by: Jen_Moderator at: 09/21/2022 10:51:18Links removed and all files added as a zip file. |
|
Follow us on