1/4/2018 11:28 AM | |
Posts: 2 Rating: (0) |
Hi everyone I want to acquire some temperature measurements from thermocouple units, monitor and project them on a monitor. Number of thermocouples are about 40 and they are K type. The distance between thermocpules and PLC is more than 20 meters. 1. Can I connect home PC to the PLC? What specifications should PLC have? What specifications should PC have? Do all PLCs have ethernet connection to be connected to PLC? If I could monitor the measurements, could I change the PLC's parameters? 2. [snip]... Thank you in advance --------------- |
Last edited by: CS Moderator at: 1/6/2018 12:10:48 PMseparat questions into different threads |
|
Follow us on