3/12/2011 5:56 AM | |
Posts: 2 Rating:
|
Hello, I'm using cp 340 RS232C module with EPSON LX-300+II printer. (PLC used is S7-300 CPU313-6BF03-0AB0). I tried the example given in the CP_PTP_PARAM cd. when i triggered M 1.0 as given in the example, TXD and RXD indicators at cp340 blinking. But, print job is not proceeded. At this stage i also checked with Hyperterminal and free serial port monitor and they also do not indicated any data transmission. Cable was ok when connected with the pc. Pls find the example program with the attachment. Thnx. Splitted from CP 340 RS 232 can be connected to all kind of Printer?. AttachmentCP 340 Getting Started Printer.pdf (96 Downloads) |
Last edited by: O_Moderator at: 3/14/2011 8:29 AMnew subject after splitting |
|
3/14/2011 8:30 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread CP340 communication problem with printer. Best regards O_Moderator |
Follow us on