9/25/2012 9:42 PM | |
Joined: 9/27/2006 Last visit: 5/19/2024 Posts: 12257 Rating: (2668) |
Hello romihs; You are right, locating sample programs for the CP 341 on TIA Portal seems elusive. However, the programming tips for Modbus RTU master ( on the CP 341) that are found in this manual (in chapter 8, Editing devices and networks) seem the same as what is required in Step 7 5.5, as described in the Modbus RTU Loadable Driver manual: STEP 7 Professional V11.0 SP2 SIMATIC S7-300/S7-400 Loadable Driver for Point-to-Point CPs: MODBUS protocol, RTU format, S7 is master Hope this helps, Daniel Chartier |
9/27/2012 5:56 PM | |
Posts: 3093 Rating: (323)
|
Hello Romihs, sometimes it is hard to find what you are looking for, but nearly everything is available on the net: Modbus Master CP341 with TIA V11 sample Regards, Kaulquappe I can only get the German link even when I try to get the English one. Just change the language after opening the link. |
This contribution was helpful to2 thankful Users |
5/2/2015 12:09 PM | |
Posts: 94 Rating: (0) |
dchartier u have example for Modbus Master RTU format for CP 341-1CH02 ? |
5/4/2015 1:46 PM | |
Posts: 3093 Rating: (323)
|
Hello Info11, Regards, |
5/22/2015 2:13 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
|
Follow us on