12/8/2007 11:48 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Hi, Are you sure that FMS is used, when not then you could easily use the CP342-5 with PROFIBUS FDL... If it is used then please use the newest blocks, if you have a older version of STEP7 then you could download the newest library SIMATIC_NET_CP Library in STEP7 / NCM S7 up to V5.4 SP3 |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
12/8/2007 4:18 PM | |||
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Dear Norbert, PROFIBUS FMS is not used very offten, it was a idea to work with objects, but customers where/are not ready for such communication. And it is normally only used for DB copying. If you could choose, then please choose for the PROFIBUS FDL communication with the CP342-5 (if you have already a CP343-5 then you could use also PROFIBUS FDL). Please look also very well which communication you are using in the SIMATIC S5 CP 5431, because not all protocols could be used on the same time. It is not possible to have simultaneous operation of PROFIBUS-DP, global I/O (GP), central I/O (CP) and PROFIBUS FMS (ZI). It is possible to have simultaneous operation of PROFIBUS DP and PLC-PLC [=PROFIBUS FDL]connection. I'am not beware for a example for communicating between a S5 CP5431 and a S7 CP343-5 with PROFIBUS FMS, maybe you could find something in the handbook:
For PROFIBUS FDL there is a example on the Product Support: Commissioning and configuring an FDL connection via PROFIBUS between a SIMATIC S5 and a SIMATIC S7 |
||
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|||
12/8/2007 8:59 PM | |
Posts: 33 Rating: (2) |
Hi Late, I havent bought any components yet. Not even the S7 CPU (319-3). That's why I asked the compatibility of this CPU. The fact: At this moment there is an FMS communication between the S5 CPU. My task is to get/put some information fro this system with S7 CPU. For me there is no problem to use Profibus FDL or even FMS. The most important thing is to make this system ready till the begining of the next year. So my hands are not tight with the FMS communication. What do you thing, can I use the Profibus FDL communication on this network simultaneously with the FMS one? Can this 2 protocol working at the same time? What can you suggest to use?I want to use the easiest one! Anyway I found some information about the FMS communication between S5 and S7.. See the attached file.... It's seems very easy to configure...do not you think??? Enjoy your weekend! AttachmentFMS Sample S7 - S5.zip (249 Downloads) |
12/9/2007 6:32 AM | |
Joined: 5/19/2006 Last visit: 4/22/2024 Posts: 548 Rating: (107)
|
This info dated 1999 it refers to an old ugly mutant 400 CPU born into 300 form factory. I think Siemens has discontinued this CPU a while ago. I have not seen any information regarding 319 CPU and any problem with 343-5 FMS CP. Regarding FDL (Layer 2)protocol on Profibus this is the native protocol for DP and FMS (Layer 7) Please see the link for performance/restrictions for 5431 on FMS.
|
Follow us on