1/8/2019 8:05 AM | |
Joined: 1/20/2012 Last visit: 5/3/2024 Posts: 15 Rating: (0) |
I know the software and hardware on the issue that I'am about to bring up is outdated, but this is somewhat my last option. I have a CP5511 profibus card to communicate to a S7 315 PLC. This works flawless for connecting Step7 to the PLC. But the problem is when I want to use it for OPC communication with the PLC, I cannot start it up in the station configuration editor. The diagnostics of the editor tells me error no 10037, and when double tapping that it mentions "please contact your siemens partner" :-) For information, I do this on a clean en new installed XP pc. Furthermore I use SIMATIC NET PC Software 2006, and the latest Step7 version. To set this all up I followed this guide with profibus. Hope anybody can help D |
Follow us on