6/6/2014 5:02 PM | |
Joined: 10/1/2013 Last visit: 5/2/2024 Posts: 605 Rating: (71) |
Hi,
In your CPUsHW config you have an option toactivate a clock memory and provide it to a Byte (e.g. MB 10). The different bits of this byte can then be used as differently clockedclock marker (2sec, 1sec, 0.5sec, ...).
DONES isTRUE when the task of your block (USEND) has been correctlyexecuted. ERROR is TRUE when the opposite of DONE happened. STATUS shows the status of the block, if an error occurs(For more information look at the online help F1) Your link leads to a description of BSEND, you might follow this link for USEND: http://support.automation.siemens.com/WW/view/en/22791526 |
6/11/2014 11:42 AM | |
Posts: 2348 Rating: (263) |
Try EN_R := True for receiving block. |
6/11/2014 12:39 PM | |
Posts: 30 Rating: (0) |
Yes, I already did that in the URCV block, or you mind somewhere else? |
6/13/2014 8:30 AM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating: (43) |
Please have a look in the following compendium: http://support.automation.siemens.com/WW/view/en/20982954 With the help of the jumping labels you can find a) the possible way how you can communicate between DP and PN CPU b) the blocks which you have to use for the communication. really helpful document, imo |
Best Regards, |
|
6/16/2014 2:12 PM | |
Posts: 2348 Rating: (263) |
Yes, i meant URCV block. What you have in status? |
6/26/2014 12:42 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
New question splitted to CPUs data exchange via PUT. Best regards O_Moderator |
6/26/2014 12:45 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
The following information was copied to here from the following closed thread Data exchange between CPU DP and PN (S7300).
|
Follow us on