12/17/2021 6:45 AM | |
Joined: 4/28/2015 Last visit: 5/22/2024 Posts: 83 Rating: (41) |
Hello Lourdes This note applies e.g. when a valid license is deactivated. An example of such a situation is when the dongle of the associated engineering license is unplugged. After that, if you were in engineering mode, you can only go back to operating mode and that's it. If you don't have a valid license, you can't really test much, because in demo mode you are very limited. So there are 2 options, either you get a demo license (Ordering details: P55802-Y140-A100 (CCA-DEMO)) or you use the SI Demo Portal (a ready-to-use Virtual Machine on the Cloud that you can book for 2 – 12h). For both options it is necessary that you contact your local Siemens organization and describe your need. Kind regards, |
Last edited by: Mucklor at: 12/17/2021 06:45:58 |
|
This contribution was helpful to1 thankful Users |
12/17/2021 3:52 PM | |
Joined: 10/21/2011 Last visit: 5/13/2024 Posts: 26 Rating: (1) |
I understand. Thanks a lot. Merry Christmas and Happy New Year. Take care Lourdes |
Follow us on