7/1/2015 6:34 AM | |
Posts: 93 Rating: (0) |
Hi all, In my program data exchange between plc and drive using SFC14 and SFC15. my program structure is FC109 used for main of drive communication that FC109 inside call SFC14 & SFC15. then that FC109 used(call) for various drive operation. i m not familiar with the function of plc to drive and vice versa. in my program FC-109,the read and write data in the array format. After that array data is spillted into various address. here i attached the FC-109 block,pls go through and guide me,that the array is how to spillted and how to determined in the specific function like that ready to run,alarm,fault,etc.,, in my program. Advance Thanks & Regards, Suryamuni. AttachmentFC109.pdf (106 Downloads) |
7/1/2015 6:36 AM | |
Posts: 93 Rating: (0) |
Hi all, here i attached the file for my doubt in details. pls go through and guide me. Regards, Suryamuni. Attachmentdrive control and status word.pptx (117 Downloads) |
Follow us on