7/5/2011 10:16 PM | |
Joined: 9/27/2006 Last visit: 10/3/2024 Posts: 12283 Rating: (2685) |
Hello A.control; To work with the Modbus drivers you need a CP PtP parametrization package: From: http://support.automation.siemens.com/WW/view/en/8713784 You need the following to be able to work with the CP PtP Modbus Master software:
Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 7/5/2011 10:17 PM |
|
7/7/2011 5:09 AM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hi A.Control, Installed the Latest Loadable Driver "Modbus Master (RTU)" V3.1 + SP6 I have also face the same problem I have updated with latest Modbus Driver & then it is working. |
Ammy |
|
7/10/2011 11:35 AM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Hi Also Check this: Modbus communication with Delta V DCSRegards |
4/3/2017 4:07 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by R.Sajjad207 is split to a separate thread with the subject What heppens when downloading modbus Slave Drivers to CP341 while CPU 315-2 DP is running?. Best regards |
Follow us on