4/14/2015 10:05 PM | |
Posts: 24 Rating:
|
Hello again. I used cable from this topic OP17 to PC When i connect OP17 to PC (ProTool) there was a messages: first "Establishing the serial connection at COM 1 with 9600 baud..." and in the end of procedure "The physical interface parameters you configured under PLC-Driver-Parameters are not allowed for the hardware version of the device currently connected" So download failed. Do i need to change anything in those parameters? look for attachment |
4/15/2015 7:30 AM | |
Joined: 8/27/2006 Last visit: 9/2/2024 Posts: 719 Rating:
|
Try to change the baud rate to 9.6 |
The more you know, The more you know that you don't know |
|
4/15/2015 1:41 PM | |
Posts: 24 Rating:
|
Ok i find it. Accordind this picture OP17-PP doesnt support PLC's S7. It is possible? |
This contribution was helpful to
1 thankful Users |
Follow us on