10/28/2022 5:12 AM | |
Joined: 5/9/2022 Last visit: 5/7/2024 Posts: 1 Rating:
|
Hi I'm testing F-I/O via ertec200p-2(starterkit) with s7-317f-2 pn/dp (TIA-Portal v17). and here is two questions. 1) when I stop PROFIsafe device driver and application. F-I/O passivated and I can read this message from Diagnostics buffer(check attached screenshot). I think this is normal response but CPU didn't stop. Is this normal operation?? or Did I miss something? 2)PROFINET Cycle time can be adjusted by "Update time". I verified this by wireshark. but PNIO_cbf_trigger_io_exchange() function always run every 1 msec. this is weired.. because this callback function should be executed, when the transmission of IO data has been finished. plz let me know if more information need.. thanks in advance. Moonsun Attachmentpassivated_ioCycle.zip (241 Downloads) |
Last edited by: mspark at: 10/28/2022 05:14:02 |
|
Follow us on