10/6/2013 2:25 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, The older CPU/CPs you mention have firmwares where S7 redundant connections were based upon ISO. The newer CPU/CPs allow both (ISO and IP based with ISO-om-TCP). To interconnect older and newer systrems, be sure you have checked the "Set MAC address-Use ISO" property of the CPs. Assign a unique MAC to each CP (changing the most right digits). See screenshot in annex. AttachmentSet MAC address-Use ISO.zip (175 Downloads) |
Best regards |
|
Follow us on