11/26/2020 12:07 PM | |
Joined: 4/26/2019 Last visit: 4/17/2024 Posts: 4 Rating: (0) |
Have the same problem with the SQL version V20 which it has roughly 1 week old https://support.industry.siemens.com/cs/es/es/view/109779336/en For the moment im trying with commenting the TRCV block at line 371. If some of you have a proper fix for the V20 please tell us. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/26/2020 12:29:25New subject after splitting Last edited by: Jen_Moderator at: 11/26/2020 12:31:45Optimized link. Last edited by: DMPEF at: 11/26/2020 13:48:10Last edited by: DMPEF at: 11/26/2020 13:48:25 |
|
11/26/2020 1:30 PM | |||
Joined: 4/26/2019 Last visit: 4/17/2024 Posts: 4 Rating: (0) |
Thanks moderator for creating the topic. The problem is: Enable SQL server and TRCV gives me error 8088 (see video here: [snip]) After trying to fix it, I cancelled the TRCV in line 371 of the FB and forced the code to enter to the "datarecieved" if statement. The result is, SQL connection established succesful and I can even WRITE to my SQL server with absolutely no trouble. But of course, I can't read any data since I commented the code of it. When I uncomment I get the 8088 TRCV error back, instantly without even executing a SQL command (just with the enableSQL)
AttachmentksF5kjy.zip (37 Downloads) |
||
Last edited by: DMPEF at: 11/26/2020 13:30:35Last edited by: DMPEF at: 11/26/2020 14:01:20Last edited by: Jen_Moderator at: 11/26/2020 14:07:11Removed link and added file as an attachment. |
|||
This contribution was helpful to1 thankful Users |
Follow us on