11/26/2018 9:37 AM | |
Joined: 8/3/2009 Last visit: 5/27/2024 Posts: 12984 Rating: (1653) |
Hello mithir.2286 Yes you can use SNAP7 for example. If you have a S71500 PLc for example then you could also use a OPC UA Connection: Here a little example: https://support.industry.siemens.com/cs/de/en/view/109737901 Bye Murof |
If this Information really helps, you could use the Rate function |
|
11/27/2018 12:35 PM | |
Posts: 4 Rating: (0) |
Yes i already done this setting in TIA Portal in Project Block and Attribute. |
3/28/2019 6:18 AM | |
Posts: 4 Rating: (0) |
IS There any Card i need to install in PLC Or I can directly read data using Ethernet port is available in PLC? |
Follow us on