11/14/2023 6:13 AM | |
Joined: 1/21/2013 Last visit: 5/20/2024 Posts: 2798 Rating: (452) |
Hi Mudhar, Resetting the panel usually means performing a factory reset. In your case, however, you need the original project to proceed. A full backup of the device includes the device settings, including the secure mode settings. The configured password is required to disable secure mode. If no password is configured, simply click the "Taskbar" button. Kind regards |
11/14/2023 7:16 AM | |
Joined: 2/18/2021 Last visit: 3/27/2024 Posts: 8 Rating: (0) |
Hello Stefan Thank you for your reply well, my problem is that I don't have the project files (engineering files). I have an old engineering project provided by the customer. If there is no hope on removing the secure mode, i will have to download the old project to the HMI and try to find the differences and add them if required. I still hope that there is a way to remove the Secure mode. maybe using a bootable USB stick with and removing the secure mode? is there such a possibility? |
Follow us on