10/4/2020 9:52 AM | |
Posts: 25 Rating:
|
Hi Is there any way to separate these ports, Yes having the same ID but not connected together. To clarify my question let me explain our system, as attached files our system consist of two redundant CPU S7-412 H, 2 SCALANCE XC206-2 Switches (6GK5206-2BB00-2AC2) and one HMI TP 1500 Comfort, The system connect to DCS through 2 redundant fiber optic cable. The redundant of HMI was working very well but after connect the DCS fiber optic cables to the switches the HMI become slow in show Feed back and receive order, also the DCS System Engineer inform us that our system make conflict at DCS system. So now we removed one ethernet cable of two cables connected to HMI then no problem in HMI (slow in Feed back) and no conflict at DCS system but now the HMI connect to CPU1 only. I follow all instruction from Siemens support in same link for establish HMI redundancy. And as I mentioned before it was working very good, but all problem happen after connect DCS. Ethernet cable was connect to HMI as per attached file X1 (P1 & P2). So I think If I separate these two ports, the problem will be solve. Some one suggest to activate Media redundancy for HMI Port but it show me that I have to use it as client and If I select Clint it show me error ( a manger must be configured ). So I add a temporary switch and made it as a manager then make HMI port X1 as MDR client, but also still the same problem. in below YouTube link I upload a recorded video Of HMI showing blinking of both tags (TRIGGER_PLC1 and TRIGGER_PLC2) First in case no connection to DCS then I will connect the DCS Then remove DCS Connection again. https://www.youtube.com/watch?v=fKdekcx81uE&feature=youtu.be I tried to put all details in attached file as possible. Thanks in advance.
------------------------------------------------------------------------------------------ AttachmentSystem.zip (49 Downloads) |
Last edited by: Jen_Moderator at: 10/05/2020 11:29:55New subject after splitting |
|
10/5/2020 11:30 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
The second thread with the subject HMI slow in Feed back when two ethernet cables are connected to it is published within the conference SIMATIC Panel. Best regards,Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on