10/5/2018 5:59 AM | |
Joined: 7/21/2018 Last visit: 6/23/2022 Posts: 53 Rating:
|
Dear Everyone, i have error with HMI TP1900 COMFORT .i have file source hmi from winccflexible convert to tiaportal V13,after that iRUNTIMEon Tia V13 is ok.when i dowload to HMI TP1900 confortvalve item flashcontinuous. hope Everyone can help me. Regard Linh AttachmentERROR HMI.docx (41 Downloads) |
10/12/2018 10:25 AM | |
Joined: 8/3/2009 Last visit: 8/15/2024 Posts: 13561 Rating:
|
Hello together It is right that the communicaton is down, but also in the PC Screenshot, so its not the reason. -> if you do not have set the pink background of the Items then it could also be a problem with tranparency. Perhaps this one could help: https://support.industry.siemens.com/cs/ww/en/view/101167295 Bye Murof |
If this Information really helps, you could use the Rate function |
|
11/14/2018 1:58 AM | |
Joined: 7/21/2018 Last visit: 6/23/2022 Posts: 53 Rating:
|
Dear Caod. it is the connect ok.because i can control valve in the real. it just only flash item valve Thanks Linh |
11/14/2018 2:11 AM | |
Joined: 7/21/2018 Last visit: 6/23/2022 Posts: 53 Rating:
|
|
Follow us on