6/11/2019 12:23 PM | |
Joined: 9/30/2016 Last visit: 5/13/2024 Posts: 911 Rating: (6) |
Hi again Hati, Thank you helping me. Please also see the screenshots. HOW do I see it in the HW config if there is one or more I/O Link masters there? And (since The unhelping hand have decided it MUST be answered in this thread or not at all) I have to repeat: Will it work (without any migration problems) if I simply install S7-PCT v3.5 SP1 (or S7-PCT v3.5 Upd. 1 as I have that version on a DVD)?
AttachmentHW Conf.zip (108 Downloads) |
6/12/2019 2:28 PM | |
Joined: 9/30/2016 Last visit: 5/13/2024 Posts: 911 Rating: (6) |
Hi again Christoph, Here are some screenshots from the older ES. I can see that I am missing some HW updates - but how do I see which (I did open some of the elements with a ?)? It looks to me like some nodes are missing - like between 31 and 41 and between 49 and 56 and between some of the IM155 modules - how do I know WHAT is missing? What do I do with the "Modules - HW updates which cannot be displayed"? - that is to rectify the error it is showing?
AttachmentHW Updates.zip (117 Downloads) |
6/20/2019 12:06 PM | |
Joined: 9/30/2016 Last visit: 5/13/2024 Posts: 911 Rating: (6) |
No more answers on this subject? |
Follow us on