6/4/2019 2:55 PM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please also see the screenshots I am installing an Engineering Station with older SW versions to match a few of our machines also running older versions. I am however still getting a warning / error error that some of my sw is either too old or not installed. So - I can see I am not having S7-PCT V3.3 + HF2 - where can I find this and install it? If it is a option in a standard package just not installed yet I would also like to know this. AttachmentzES'er.zip (399 Downloads) |
Last edited by: xmnj at: 06/04/2019 15:09:28Attachment Last edited by: xmnj at: 06/04/2019 16:04:17Removed defective zip file Last edited by: xmnj at: 06/04/2019 16:05:32Last edited by: xmnj at: 06/04/2019 16:06:19Last edited by: xmnj at: 06/06/2019 06:52:24 |
|
6/4/2019 3:01 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981) |
Hello, S7 PCT is a package in the Step7 Install data. Regards Christoph |
6/4/2019 3:02 PM | |
Joined: 9/27/2006 Last visit: 5/3/2024 Posts: 12257 Rating: (2666)
|
Hello xmnj; You can download S7-PCT v3.5 SP1 from the following link: https://support.industry.siemens.com/cs/de/en/view/32469496 S7-PCT v3.3 HF2 was made available in 2016, and it is replaced now by this latest version. If you really need v3.3, you should try contacting your nearest Siemens rep, maybe he can ask for the v3.3 files from Siemens for you. Hope this helps, Daniel Chartier |
6/4/2019 3:14 PM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Hi Christoph and Daniel and thank you for answering. Christoph: So I can use the SR4 DVD my coworker dug out for me and find the S7-PCT V3.3 on that - and do a partial install? Daniel: Please see the NOW attached screenshots and tell me if S7-PCT v3.5 SP1 is compatible with the rest of the SW on the new ES. Would it not be better to use the same version as is installed on the "old and working ES"?
|
6/6/2019 7:13 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Hi again Christoph and Daniel, I have tried zipping the .docx file with the 2 pics and attaching it again. What the screenshots show is that a working ES has S7-PCT V3.3 (HF2) installed but my new (not working) ES only has S7-PCT V3.2 installed. S7-PCT V3.2 IS the version contained in the S7 SR4 DVD used. Which DVD can I find S7-PCT V3.3 (HF2) on? Will it work (without any migration problems) if I simply install S7-PCT v3.5 SP1 (or S7-PCT v3.5 Upd. 1 as I have that version on a DVD)?
AttachmentAES'er.zip (258 Downloads) |
6/11/2019 10:14 AM | |
Joined: 9/21/2012 Last visit: 5/3/2024 Posts: 3937 Rating: (444) |
PCT is only for Siemens IO-Link master configuration. Does your project have Siemens IO-Link masters? |
Follow us on