5/4/2018 10:34 AM | |
Posts: 531 Rating:
|
I think he wants to know how to change the ip of 1 cp and only upload to one device, not to all devices?!? |
5/4/2018 3:27 PM | |
Joined: 11/19/2015 Last visit: 6/13/2024 Posts: 4 Rating:
|
Hi Murof, I m very thankful to you for reply, I have attached here pdf of Netpro, hope this is clear to view, in network u can see there are 3 GTG and 1 Other station (DCS) are configured with my system through modbus Tcp/IP with address their addess 192.168.1.223 -------232, and 192.168.1.201 But now they are saying that they have different IP address which is 10.0.1.11---------42. for all 3 GTG and DCS system. so my question is ' How to change the ip address of the particular CP which is connected with GTG and DCS" Should I have to change the all address (from 192.168.1.11......... TO 10.0.1.11..........)of my all plc Modules and how to download the whole changes in plc I have very little bit knowledge about this s7 400H system please guide me . AttachmentPr.pdf (98 Downloads) |
Follow us on