12/31/2022 6:52 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (819)
|
Hello,
if you tell us what comm protocol is used or available via ETH interface then it can be better clear. Check carefully documentation about your device and comm modules. Without to know is hard to help clearly. Link to manufacturer ETH module: Link to IME ETH module spec From quick view is clear probably that Modbus RTU and Modbus TCP or Modbus RTU over TCP is used. Check documentations in link. If this is correct then you need programm communication via available blocks inside TIA portal and no add any HW cfg as PN or PB DP in this case is required. |
Last edited by: Duris_I at: 12/31/2022 07:03:01Last edited by: Duris_I at: 12/31/2022 07:04:49With best regards... |
|
Follow us on