3/9/2011 12:54 PM | |
Posts: 153 Rating: (15) |
Hi_darkduino Such decisions can be realized on the device in the different ways: 1)To 10 meters LOGO TD Panel + logo with modular expansion modules 2)To use 2 LOGOwith modular expansion modules https://www.automation.siemens.com/tf/WW/en/Posts/48301#top Or the last message https://www.automation.siemens.com/tf/WW/en/Posts/44935#top 3)To use the communication module for EIB/KNX or AS-i 4) Via ethernet (Soon) |
3/9/2011 1:51 PM | |
Posts: 4 Rating: (0) |
Thank you for your help. I jnow I have to buy a EIB bus to make connection for 2 LOGGO but I'm not sure about what model? And I don't know how to connect it? |
3/9/2011 3:22 PM | |
Posts: 4 Rating: (0) |
So everything is already wired in the logo. Input, they are buttons. Output lamps, at least for the moment. Simply, it is a logo with 20 entries and another with 16 entries. For now, I've programmed the first logo. It cuts the light output which is the first logo. I want that pressing this button (which enters the first logo), lighting the entire building (including so what is the output on the second LOGO) In the diagram you sent me, I have the modules 1 and 2, I'll have to buy the module is 3 but I have to buy 4 as to connect the 2 LOGO? http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=21688364&caller=view Thank you |
3/14/2011 5:06 PM | |
Posts: 4 Rating: (0) |
Thank you very much for all that information |
Follow us on