4/7/2015 9:50 PM | |
Joined: 11/6/2009 Last visit: 10/18/2024 Posts: 13 Rating: (0) |
Hello, I am trying to migrate a program from S7 300 to S7 1500. The program needs to create a connection to a PC and then send and receive data from the PC. I managed to create a connection using the TCON FB with a TCON_IP_v4 data type. I tried to use the TCON_PARAM data type (like it was used for the 300 PLC) but I could not establish an active connetion this way with the 1511 PLC For the HardwareID I used 64 which is the hardware identifier address of the profinet interface (for the 300 the profinet number was used for example if the cable was connected at the X2 port then I used 2 as the hardware ID). As far as the local defined instace of TCON_IP_V4 or a dedicated DB , I had the same result with both. My question is which parameter is better to use with TCON FB for 1500? Thank you Micky
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 4/9/2015 1:04:30 PMNew subject after splitting |
|
Follow us on