6/30/2009 4:12 PM | |
Joined: 5/8/2006 Last visit: 10/16/2024 Posts: 1085 Rating: (77) |
Hi does this phenomenon appears with an new panel, tooor only after 6 month? - A problem can be electrical or magnetic fields of high intensity! - vibrations |
7/3/2009 8:23 AM | |
Posts: 38 Rating: (0) |
Hello ZAK, till now, it was repeatable: we exchanged the panel, the image on the new panel was OK, after some period (6 months) the image started to "flicker". Although we use electric fields (for welding), they are not active near the machine - it's a press and it's in complete different part of the factory. Nevertheless, I tried to move the erroneous panel completely outside, and the distortions were there, too - so it looks like it's not dependent on magnetic field. We will definitively try to reduce the vibrations - but completely eliminate them is not possible, the machine is press and it simply creates big vibrations during work. On the other hand, we received a notice from Siemens, that all 377 panels with serial number lower than 4 can have "sporadic problems". So we will once again exchange the panel, add a rubber isolation and wait what happens... Thank you all for your valuable comments. Have a nice day. Petr |
9/27/2017 7:15 PM | |
Joined: 1/4/2013 Last visit: 8/30/2024 Posts: 1 Rating: (0) |
Was anyone able to come up with a solution to this distortion problem? I have 2 MP377 19" with the same problem! |
Follow us on